• Connect

Education

Welcome to your online source for lighting enlightenment and lighting industry education. Enhance your knowledge of lighting, and discover professional learning opportunities.

BIM: Frequently Asked Questions

What is the difference between BIM and Revit?

BIM (Building Information Modeling) is an intelligent, 3D model-based process for planning, design, construction and management...

Read Full Answer

BIM (Building Information Modeling) is an intelligent, 3-D model-based process for planning, design, construction and management of buildings and infrastructure. Revit is one of the BIM platforms (software packages) used to create BIM models.

What is a Revit file?

A Revit file is the output from the software. It can be in one of three formats:

Read Full Answer

A Revit file is the output from the software. It can be in one of three formats: RTE (Revit Template File), RFA (Revit Family File), RVT (Revit Project File).

Why does an LED Revit family emit various colors in a rendering?

This is the result of the IES file(s):

Read Full Answer

This is the result of the IES file(s):

Revit seems to have an issue with "reading" absolute IES files for LED lighting fixtures. The IES file notes a "-1" for the initial lumens value.

A discretionary approach is to change the "-1" to the initial lumen value of the LED lighting fixture, save (you may want to add characters to the end of the filename to differentiate it from the original IES file) and reload the IES file in the Photometric Web File parameter.

What is a type catalog?

A type catalog (comma-delimited text file (.txt)) is an external file that contains specified syntax for family types and parameters...

Read Full Answer

A type catalog (comma-delimited text file (.txt)) is an external file that contains specified syntax for family types and parameters. It is best practice to keep the list of family types within the model to six or less. If more are needed, a type catalog with specified syntax should be created.

The type catalog file must be in the same folder and location and have the same file name as the corresponding Revit family; if not, the types and data will not load into a project file.

How do I load a Revit family that has a type catalog into a project file?

From your project file, click Load Family located under the Insert menu.

Read Full Answer

From your project file, click Load Family located under the Insert menu.

Does Eaton’s lighting division provide 2D CAD files of its products?

Eaton's lighting division provides 2D CAD files of products by request.

Read Full Answer

At this time, we only provide 2D CAD files of products by request. If you need a more detailed 2D CAD drawing (similar to what’s shown in a specification sheet), our engineering department can address your request.

How can I reach someone at your company who can help me with your Revit files?

Learn how to get answers to your questions regarding Eaton's Revit files.

Read Full Answer

We have a few different ways that you can get your questions answered regarding our Revit files. Your questions will be addressed by our in-house BIM manager. 1) Send an email to LightingBIM@Eaton.com; 2) Contact us using this form and select BIM / Revit from the list in the ‘You have a question about’ field; 3) Submit a question in our nano request question field pop-up window located at the bottom left of the Eaton’slighting division website.

What are the benefits of BIM?

BIM is an intelligent, model-based process that makes it possible for many different stakeholders to work more collaboratively.

Read Full Answer

BIM is an intelligent, model-based process that makes it possible for many different stakeholders to work more collaboratively and more effectively. The transfer of knowledge is streamlined to assist with the planning, designing, building and managing of buildings and infrastructure. BIM models are actionable, and they reduce errors and reworks. They are also accessible anywhere and anytime.